FB#.SINGLETURNBITS

Description

Number of single turn bits used for BiSSClosed"Bi-directional Serial Synchronous interface" An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder rotary encoders. Feedback data sheet should specify the number required.

Context

Only used for when FB#.MECHTYPE is rotary and identified feedback is BiSS. See Feedback Devices.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

single turn bits

Range

1 to 32

Default Value

19

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.